How to mitigate interference between multiple LiDAR sensors?
Answer:Interference between multiple LiDAR sensors can be mitigated or even avoided by adding PhaseLock function to the LiDAR or optimizing the LiDAR mounting position.
Is the LiDAR laser harmful to human eyes?
Answer:RoboSense LiDAR sensors are certificated with class 1 eye safety according to the IEC/EN 60825-1:2014 standard, which means they are safe under all conditions of normal use.
What’s the wavelength of the RS-LiDAR?
Answer:905nm.