How to mitigate interference between multiple LiDAR sensors?
                
                Answer:Interference between multiple LiDAR sensors can be mitigated or even avoided by adding PhaseLock function to the LiDAR or optimizing the LiDAR mounting position.
              
            Does RoboSense provide time synchronization board for time synchronization of multiple LiDAR sensors?
                
                Answer:Yes. The time synchronization board is sold as part of RoboSense’s LiDAR perception solutions, please check with your account manager for a quotation.
              
            Is the LiDAR laser harmful to human eyes?
                
                Answer:RoboSense LiDAR sensors are certificated with class 1 eye safety according to the IEC/EN 60825-1:2014 standard, which means they are safe under all conditions of normal use.
              
            After synchronized with GPS, the UTC time of the point cloud of the LiDAR is 1s or 1s+1 PPS pulse width lagged behind the actual time.
                
                Answer:Currently, this problem only presents in the RS-LiDAR-16, RS-LiDAR-32 and RS-BPearl products. Other products do not have such problem.
(1)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 255 or 0 (Check through RSVIEW-TOOLS-RSLidar info), there will be a lag of 1S+1 PPS pulse width;
(2)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 1, there will be a lag of 1S;
(3)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 2, the time is synchronized with the current time of GPRMC;
(4)The V3.0 and earlier version of the RS-LiDAR-16, and the V1.7 and earlier version of the RS-Lidar-32 do not support time mode setting;
            (1)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 255 or 0 (Check through RSVIEW-TOOLS-RSLidar info), there will be a lag of 1S+1 PPS pulse width;
(2)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 1, there will be a lag of 1S;
(3)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 2, the time is synchronized with the current time of GPRMC;
(4)The V3.0 and earlier version of the RS-LiDAR-16, and the V1.7 and earlier version of the RS-Lidar-32 do not support time mode setting;
Does the LiDAR currently support Beidou time synchronization?
                
                Answer:Not at the moment. If necessary, please contact RoboSense technical expert to evaluate the feasibility and cost.
              
            Will there be a delay after the LiDAR receives a GPS time synchronization signal?
                
                Answer:No.
              
            What are the requirements for the power supply?
                
                Answer:
(1) The power supply should be stable;
(2) The power supply and current should be able to support stable operation of the LiDAR;
(3) The power supply shall provide sufficient starting current for the LiDAR;
            (1) The power supply should be stable;
(2) The power supply and current should be able to support stable operation of the LiDAR;
(3) The power supply shall provide sufficient starting current for the LiDAR;
When connected to the pluggable space-style bayonet connector, are the LiDAR sensor itself and the interface box waterproof?
                
                Answer:The LiDAR sensor itself is waterproof, but the interface box is not.
              
            LiDAR restarts repeatedly or the rotating motor do not start?
                
                Answer:Check the current and voltage output. If you are using modified or extended cable, please also check the voltage drop.
              
            Is the pluggable space-style bayonet connector waterproof?
                
                Answer:The connect of RS-LiDAR-16 before v4.0 and that of the RS-LiDAR-32 before v2.0 are not waterproof.
              
            When LiDAR is screwed tight to a platform, the point cloud is rotating.
                
                Answer:The rotating point cloud is due to repeated restart of the LiDAR. If the screw is too tight or the mounting platform is not flat, the stressed will change the ideal space between the code disc and the encoder in the LiDAR, resulting in the zero point cannot be recognized and therefore the repeated restart of the LiDAR.
              
            What causes the loss of certain angle data of the point cloud.
                
                Answer:This might be due to a host computer that loses packets. Please check the host computer CPU and memory occupancy, or the network load and network status.
              
            Will 2 LiDAR sensors shooting at each other affect the point cloud quality?
                
                Answer:For LiDAR sensors using lasers of the same wavelength and without anti-interference function, there will be noise in the point cloud. Mechanical LiDAR with PhaseLock function can effectively avoid interference without affecting the quality of point cloud.
              
            At a sharp turn or an emergency braking, why there will be
                
                Answer:This is a normal phenomenon. Framing is done at a fixed-angle, when there is a sharp turn or an emergency braking, the framing angle will fluctuate (the angle of a UDP packet), visually, there will be gaps or overlaps of point cloud at the framing angle, nevertheless, the point cloud data is not lost.
              
            What’s the wavelength of the RS-LiDAR?
                
                Answer:905nm.