What are the requirements for the power supply?
Answer:
(1) The power supply should be stable;
(2) The power supply and current should be able to support stable operation of the LiDAR;
(3) The power supply shall provide sufficient starting current for the LiDAR;
When connected to the pluggable space-style bayonet connector, are the LiDAR sensor itself and the interface box waterproof?
Answer:The LiDAR sensor itself is waterproof, but the interface box is not.
LiDAR restarts repeatedly or the rotating motor do not start?
Answer:Check the current and voltage output. If you are using modified or extended cable, please also check the voltage drop.
Is the pluggable space-style bayonet connector waterproof?
Answer:The connect of RS-LiDAR-16 before v4.0 and that of the RS-LiDAR-32 before v2.0 are not waterproof.