Does RoboSense provide time synchronization board for time synchronization of multiple LiDAR sensors?
Answer:Yes. The time synchronization board is sold as part of RoboSense’s LiDAR perception solutions, please check with your account manager for a quotation.
After synchronized with GPS, the UTC time of the point cloud of the LiDAR is 1s or 1s+1 PPS pulse width lagged behind the actual time.
Answer:Currently, this problem only presents in the RS-LiDAR-16, RS-LiDAR-32 and RS-BPearl products. Other products do not have such problem.
(1)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 255 or 0 (Check through RSVIEW-TOOLS-RSLidar info), there will be a lag of 1S+1 PPS pulse width;
(2)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 1, there will be a lag of 1S;
(3)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 2, the time is synchronized with the current time of GPRMC;
(4)The V3.0 and earlier version of the RS-LiDAR-16, and the V1.7 and earlier version of the RS-Lidar-32 do not support time mode setting;
Does the LiDAR currently support Beidou time synchronization?
Answer:Not at the moment. If necessary, please contact RoboSense technical expert to evaluate the feasibility and cost.
Will there be a delay after the LiDAR receives a GPS time synchronization signal?
Answer:No.